I would like to use the DS90UB903/904 with a QVGA display. Unfortunately the typical pixel clock frequency of this display is specified with 6.4MHz which is below the min. 10MHz for the Serializer. Increase the frequency to 12MHz is working using cables < 2m. Unfortunately I need a cable length of 10m. Increasing the pixel clock further (> 30MHz) is not an option as the display will not display pixels correctly anymore. Is there any other way around this problem?