Other Parts Discussed in Thread: DS92LV0411, DS15BA101, DS15EA101, DS92LV0422
Hi, I'm disty of Japan area.
Please help me.
My customer is considering LVDS Ser/Des.
Application is Laser Printer.
Image size is QVGA.
Transmission distance is 0.5m.
P-Clock is 5~15MHz.
Is it possible for <DS92LV0411/0412> to transmit QVGA signal?
Thier concern is that target application of <DS92LV0411/0412> is XGA or SVGA.
In this case, P-Clock is 5MHz(min).
They are afraid of signal transmission QVGA whether <DS92LV0411/0412> can realize.
I'm waiting for your reply.
Best regards.