Other Parts Discussed in Thread: SN6501, TPS55010
I need a low cost, low power (50mA) isolated power supply. The SN6501 looks great, but I have trouble finding an isolation transformer for output voltages >5V. I think that with a primary side voltage of 5V +-2% and a secondary side voltage of 15V + headroom for a LDO on the isolated side I need a 1:3.3 transformer. Coincidentally this is the turn ratio of ADSL transformer. But are they really suitable?