Other Parts Discussed in Thread: DP83640, DP83620
On a new PCB we are using the TI DP83640 Eth PHY. On this PHY we are using the LED SPEED output (connected to the yellow led in the RJ45 connector). According to the datasheet, the output indicates that the link is operating in 100 Mbit/s mode (yellow led on) or in 10Mbit/s mode (led off). This works fine. (this also means that the strapping options, led polarity, etc are handled properly).
However we also observe the following unexpected behavior: when the RJ45 cable is NOT connected, the yellow led is still ON.
Although this is not really a violation of what is in the datasheet (There is no description in the datasheet of what happens when the link is down), it is a bit unlogical and it is different from what most other PHYs are doing (speed led off when cable removed).
Could someone confirm this behavior?