Other Parts Discussed in Thread: PROFIBUS, ISO1176T, ISO1050
Hi,
can I use the 1176T for Modbus-RTU ? I need some ESD protection as well so I added TVS diodes.
Could somone please review my RS485 circuit?
Is the resistor value of R401 & R403 correct? I know that profibus requires 220R but a value of 390~600R should be ok for Modbus / RS485?
Is the CAN circuit good too ?
My Bus Settings are:
1) 115kbaud
2) max. 32 Slaves (typical 4-8)
3) cable 50 meter length
4) Shielded twisted pair
Kind regards
E.G.