Other Parts Discussed in Thread: XIO2001
Hi,
we have a design which used the xio2001 as the pci-pciE bridge between dm648 and dm8168. the clock speed in pci side in xio2001 was set to 33Mhz, the design works fine for a long time, but recently when we build more boards, we found some of the boards has data mismatch when senting/receiving data from XIO2001 to dm648 through PCI interface, the overall chance is not high but still exists, the percentage is around 5%. When we set the clock speed to 66Mhz, this data mismatch seems not happen. I am wondering if the XIO2001 can work with dm648 with 33Mhz PCI clock. Or there is some points I should pay attention to when XIO2001 is set in 33Mhz PCI clock?
Thanks,
JK