Other Parts Discussed in Thread: TSB81BA3E
Hello,
I have system that includes two repeater boards connected as part of a system, both of which using the TSB81BA3E phy.I can confirm that they both adhere to the TI recommended termination networks in the data sheet.
If the first repeater is always powered and I then cycle power on the second repeater (as might happen in my system initially) while scoping the TPB pins, I observe that the TPB pair starts toning and then turns off and is pulled to 1.86V.
Cycling power on the second repeater does not change the state of these TPB pins (other than being pulled up to 1.86V). If I remove the 1394 connector from while observing these pins (with the second repeater powered or un-powered) they start toning again as soon as the plug is pulled.
Its obviously a power-up sequencing issue, but I don't quite understand what mechanism would cause the TSB81BA3E to disable toning and tri-state the TPB outputs. I also don't understand why disconnecting the now tristated TPB pair from the other TPA termination restores TPB operation.
I would appreciate any information you could provide on what would cause this behaviour in the PHY so I can work backwards to come up with a system cause and solution.
Thanks,
Mitch