Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PDB Timing requirement for DS90UB913A/914A

Hi TI,

Can we use PDB pin in DS90UB913/914 as reset pin? 

According to the datasheet, It recommend to use a external RC network to ensure PDB arrives after all the VDD has stabilized.   Is there any recommended value for RC? 

If I drive PDB pin using a LOW pulse as a hot reset, What is the mimimum pulse width to reset the chip effectively?  1us is OK?

Thanks & Best Regards!

Tony

  • Tony

    PDB will reset register values to their default states, and will reset the state of the PLLs, but it also powers down many portions of the chip, and as a result the timing will be quite slow.   I would feel more comfortable with a PDB time which was comparable to the lock time on the deserializer, which is on the order of 10ms.

    A much easier and faster way to reset the chips is via one of the reset bits in the Power and Reset register.

    Mark