This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

USB3.0 LPM - Achieving A Reduced-power Bus State



I'm looking for a way to cause an external USB3.0 device, such as an
HDD, to enter and exit the reduced-power USB mode (e.g., leave/enter the
U0 power state) for bus-testing purposes.

Presumably, all that is needed to be done is to set the Power Options on
the Windows Control Panel to cause hard disks in the system to turn off
after being idle for e.g. 1 minute.  However, using a Win-7/64-bit
laptop with a USB3.0 controller card and an external HDD having a USB3.0
interface, monitoring the USB3.0 bus showed that the usual background
bus activity never ceased (e.g., after 1 minute).  Note the
possibly-important detail that there is a USB3.0 hub present between the
host controller card and the HDD, with the analyzer connected between
the hub and the HDD.

I have heard that there is or might be a USB3.0 LPM software utility
that (presumably) could be used to command (or request) the USB3.0
controller to put the link(s) out to the HDD into a non-U0 state, but I
have not seen references to same on the Internet.

Any help would be appreciated.  What would be
sufficient, if no such handy utility application exists, is information
regarding what host system (brand/manufacturer) running what version of
Windows, and what USB3.0 device (brand/manufacturer), are all known to
be able to work together such that the device can be caused to enter
(and later leave) reduced-power bus mode.

  • You are looking for the usblpm.exe tool from Microsoft.  It tests low power modes and lets you see the current power states of everything on the USB.  It runs on Windows 8 and up. 

    Windows 7 systems require custom USB 3.0 drivers provided by each XHCI host controller manufacturer so USB 3.0 low power mode support will vary from system to system.

    Regards,

    JMMN