This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB 3410 Driver, Why two setups?

Hi,

the actual TUSB 3410 driver 6.7.2.0 has two setups and each neets to be executed. The fist setup unpacks that driver to the folder "c:\Program Files (x86)\Texas Instruments Inc\TI_WDF_USBUART_SINGLE_DRIVER_V6.7.2.0_WHQL\"
 and the setup in that folder installs the driver to "c:\Windows\tiinst\".

Why two setups? The old driver 6.7.1.x and 6.5 had only one setup and are more user friendly. Is there are a possibility to get a 6.7.2.0 driver with only ONE setup?

Regards

Stefan