Other Parts Discussed in Thread: TUSB1210
Hello,
I have a few questions with using TUSB1210 in the device implementation. I plan on using the ULPI input clock mode configuration and the device will be self-powered.
1. In a self-powered device configuration, do I still need to connect the VBUS pin on TUSB1210 to the +5V on the USB connector (pin 1)? If so, how does TUSB1210 use the input? Is it only an indicator or does it actually draw current from the +5V bus?
2. Should the TUSB1210 ground connections be common with the ground on the USB connector (pin 4)?
3. Beside Figure 10.2 in the TUSB1210 datasheet, are there any other reference designs for using TUSB1210 in a device configuration?
Thanks,
Noah