Is it ok to have serializer io at 2.8 and deserializer io at 3.3V ?  I am presuming CML rx, tx doesn't care about this and runs on 1.8V.
I am running the camera with the imager clock as source.
If no camera imager clock is there I2C through back channel?
If no imager clock does serializer gernerate one?
In bist mode if there is no imager clock does the serializer generate one?
Can the bist be initiated via hardware bist enable on the deserializer?
Does back channel tell the serializer to enter bist mode?  
Can bist test be initated solely with a jumper on the bist pin on the deserializer to test the link?  I would prefer no software required to see if link is good.
Should pll lock light go on in bist mode ?
If all zero data bist should work fine, correct?
Is mode ignored in bist?  I have the bist set at 50 \MHz gpio\[1:0]=10, line rate is 695.41MHz.
Bit rate doesn't seem to change between bist gpio\[1:0]=10 (50Mhz) and gpio\[1:0]=01 (25MHz) as a function of bist frequency.  But the eye closes for bist 01.  Why would that be ?
Line rate bist 12.5MHz is 353.6MHz
Finally, I have some eye patterns to discuss.  I am not passing bist at 25MHz and 12.5MHz.  I am set up for imager (pclk) as clock source.  I am not providing a imager clock during the bist tests.   I get solid pass at 50MHz but I never see a lock light.