This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TSB81BA3E optical implementation question

Other Parts Discussed in Thread: TSB81BA3E

Hi,

After solving my common mode problem between two PHY's on isolated grounds, I am on to my next question as I finish my 1394 optical repeater design.

I am pretty much following the guidance in the TI application note sgza001a but I have a question related to the turn on time of the optical TX following de-assertion of the TX-DISABLE. All optical transceivers I am considering specify a maximum of 1ms between removing tx disable and 90% optical power. I have measured actual times of between 20uS and 200uS in practice for various transceivers. This has the effect of reducing the toning intervals from 667uS to a duration of 467uS or so in the case of a 200uS delay. If a transceiver truly has a 1ms delay, there would be no toning period transmitted.

The question is: What is the minimum duration of a toning burst that is considered valid by the TSB81Ba3e phy? Any practical insight into this issue would be appreciated.

Thanks,

Mitch