Other Parts Discussed in Thread: TUSB7340
Hi,
I am using TUSB7340EVM board with fedora 19 machine which have 3.9 kernel.
The kernel is able to detect the USB 2.0 pen drive as shown below logs but the USB3.0 pen drive is not detected by the system (no logs).
I am providing 5v 18A external power supply to PCI card, jumper J40 is populated (PCIE_3p3v and Board_303v short), Jumper J26 is populated, all LEDS D5 and D1 to D4 are on.
Did I miss any setting so that my 3.0 pen drive should detect by this card. the same pen drive is detected in some other platform without this card.
Please help me out from this trouble.
Thanks
Suresh
[root@localhost B42813]# uname -a
Linux localhost.ap.freescale.net 3.9.5-301.fc19.i686 #1 SMP Tue Jun 11 20:01:50 UTC 2013 i686 i686 i386 GNU/Linux
[root@localhost B42813]# cat /etc/issue
Fedora release 19 (Schrödinger’s Cat)
Kernel \r on an \m (\l)
[root@localhost B42813]# tail -f -n1 /var/log/messages
Mar 27 06:40:10 localhost kernel: [ 6479.147969] usb 3-3: new high-speed USB device number 4 using xhci_hcd
Mar 27 06:40:10 localhost kernel: [ 6479.165896] usb 3-3: New USB device found, idVendor=0951, idProduct=1660
Mar 27 06:40:10 localhost kernel: [ 6479.165902] usb 3-3: New USB device strings: Mfr=1, Product=2, SerialNumber=3
Mar 27 06:40:10 localhost kernel: [ 6479.165905] usb 3-3: Product: DataTraveler 108
Mar 27 06:40:10 localhost kernel: [ 6479.165924] usb 3-3: Manufacturer: Kingston
Mar 27 06:40:10 localhost kernel: [ 6479.165927] usb 3-3: SerialNumber: 000FEAFB7959FC61A7D42434
Mar 27 06:40:10 localhost kernel: [ 6479.166580] usb 3-3: ep 0x81 - rounding interval to 128 microframes, ep desc says 255 microframes
Mar 27 06:40:10 localhost kernel: [ 6479.166585] usb 3-3: ep 0x2 - rounding inte