Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLK105 - inside pull resistance of configutation pins and load capacitance values

Other Parts Discussed in Thread: TLK105

Hello,

We'd like to ask TLK105.

<Question1>
After the reset of TLK105,  do inside pull UP/PD resistance of configration pins of TLK105 always(all time) connect to pull resistance?
If there are configration pins which disconnect to pull resistance after the reset, please inform us them.

<Question2>
The datasheet recommends that Load Capacitance values are from 10pF to 40pF.
Our customer uses 25MHz crystal with 8pF Load capacitance.
Can this value of Load capacitance use for TLK105' clock? 

Kind regards,

Hirotaka Matsumoto