This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83865 Transmit Issue

Hi,

I have been having an issue with transmitting data using the DP83865 PHY. I am running in 100 Mbps mode and have been able to receive data into a FPGA. Since the data comes in with the LSB first, I swap nibbles for the Ethernet block in the FPGA. The data then makes it through the Ethernet block without issue. After receiving an ARP from the computer, I can see the FPGA transmit an ARP back out on the TX[3:0] lines. I format this data the same as the receive data was coming in. However, I never see a response to the ARP from the computer when monitoring traffic using wireshark. Below is an example of received data and what I convert it to:

C5 C5 C5 C5 C5 C5 C5 C5 C5 C5 C5 C5 C5 C5 C5 CD  => 55 55 55 55 55 55 55 D5

So when I send data out, I flip the LSB and MSB since that is how it is received into the FPGA, as such:

55 55 55 55 55 55 55 D5 =>05 05 05 05 05 05 05 05 05 05 05 05 05 05 05 0D

Could you please let me know if my assumption on flipping the data before transmitted is flawed or if you have any other tips as to what I may be able to do to correct this problem?

Thanks

  • I will double check the bit order.  In the meantime, another option would be to loop the transmit data back to the FPGA and see if it is correctly received. This takes the computer on the other end of the link out of the equation.

    Internal loopback is configured via bit 14 of the BMCR register (adddress 0x00).  You will want to force the speed (as opposed to using auto-negotiation) and remove the cable from the RJ-45. 

    Patrick