Other Parts Discussed in Thread: SN65LVDS22
Dear TI
i'm Valerio from italy,
i have this datastream :
data stream outputs is an ITU-R BT.656 data stream. The ITU-R BT.656 data stream is
connected into a CSI-2 Tx module. Data from the CSI-2 Tx module is fed into a D-PHY physical layer and output serially from the device. The output consists of a single data channel on the D0P and D0N lanes and a clock
channel on the CLKP and CLKN lanes.
The data stream output video data in an 8-bit
YCrCb 4:2:2 format. The video data is output in an interlaced
format at a nominal data rate of 216 Mbps.
I need convert this datastream from single data channel D0P,D0N,CLKP,CLKN to format parallel 8 bit for connection to DM816x.
LVDS324 component texas is ok for this application?Can you send me schematics or application note with this connection?
Thanks!
Best Regards!
Vale