This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Display port / 2:1 MUX to select AUX or DDC

Guru 29720 points

Other Parts Discussed in Thread: SN74CBT3306, TS3USB221E, TS3USB221A

Hi Team,
 
My customer is looking for the device that is 2:1 MUX to select AUX or DDC.
He doesn't require the DisplayPort switch that can switch main link.
(He requires the switch that can select AUX or DDC only.)
He is also considering discrete solution, but would like to use switch IC.
The bandwidth(-3dB) of this switch requires up to 1MHz(=AUX signal frequency).
Does TI have any appropriate switch for this purpose?
 
As a trial, I searched TI devices and found SN74CBT3306(dual FET bus switch).
Is it possible to use the device for this purpose?
Your help would be appreciated.
 
Best Regards,
Yaita / Japan disty