Other Parts Discussed in Thread: PCA9545A, TCA6408A
Hi,
Is it possible INT pin to be open if customer doesn't use this pin?
I think it is OK because of open drain output, but would like to confirm just in case.
Best Regards,
Yaita
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Yaita,
Which device are you concerned with?
If you look at the link to the thread below bullet 2) offers guidance on how to handle unused INT pins for PCA9545A. There are other E2E threads like this one you can search through that may also offer guidance.
http://e2e.ti.com/support/interface/etc_interface/f/390/p/318966/1110566.aspx#1110566
Thank you,
Adam
Yaita,
Yes it is also recommended for the TCA6408A that any unused INT pins are connected to ground.
Adam