Other Parts Discussed in Thread: AM3354, DP83848M
|
We're using DP83848M on AM3354. When the LAN cable is plugged into the RJ45 port, the DP83848M is able to tell am3354 about this status change. However, the DHCP client doesn't work ! No IP address can be obtained from the DHCP server (just a simple WiFi router). Even I set a static IP address to the ethernet port, ping never succeeds, either ! We're using MII interface, PHY addr = 1, 10/100Mbps auto negotiation. Schematic in pdf is as attached. |
The followings are the registers dump :
1:phyreg[00] BMCR : 3100
1:phyreg[01] BMSR : 786d
1:phyreg[02] PHYIDR1 : 2000
1:phyreg[03] PHYIDR2 : 5c90
1:phyreg[04] ANAR : 01e1
1:phyreg[05] ANLPAR[NP] : cde1
1:phyreg[06] ANER : 000f
1:phyreg[07] ANNPTR : 2801
1:phyreg[08] RESREVED : 0000
1:phyreg[09] RESREVED : 0000
1:phyreg[0a] RESREVED : 0000
1:phyreg[0b] RESREVED : 0000
1:phyreg[0c] RESREVED : 0000
1:phyreg[0d] RESREVED : 0000
1:phyreg[0e] RESREVED : 0000
1:phyreg[0f] RESREVED : 0000
1:phyreg[10] PHYSTS : 0015
1:phyreg[11] RESREVED : 0000
1:phyreg[12] RESREVED : 2c00
1:phyreg[13] RESREVED : 0000
1:phyreg[14] FCSCR : 0000
1:phyreg[15] RECR : 0000
1:phyreg[16] PCSR : 0100
1:phyreg[17] RBR : 0001
1:phyreg[18] LEDCR : 0000
1:phyreg[19] PHYCR : 8001
1:phyreg[1a] 10BTSCR : 0804
1:phyreg[1b] CDCTRL1 : 0000
1:phyreg[1c] RESREVED : 0000
1:phyreg[1d] EDCR : 6011
1:phyreg[1e] RESREVED : 083e
1:phyreg[1f] RESREVED : 0000
Any possible cause of the problem ?
Looking forward to any advice ! Thanks !