Other Parts Discussed in Thread: DS90CF384, DS92LV2412, DS92LV2411
customer identified that the major cause of their EMI problems comes from the LVDS to RGB IC DS90CF384
Can you find a replacement with spread spectrum capability?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: DS90CF384, DS92LV2412, DS92LV2411
customer identified that the major cause of their EMI problems comes from the LVDS to RGB IC DS90CF384
Can you find a replacement with spread spectrum capability?
Hi Eli,
Somebody is looking into this and will respond shortly.
Regards,
Michael Peffers
High Speed Interface Applications
Hi Eli,
The DS90CF384 is an FPD I generation device, and unfortunately we do not have any LVDS-RGB ICs in our portfolio that can perform the spread spectrum clock generator (SSCG) function and is a drop-in replacement for the DS90CF384.
I would advise if SSC is a major concern and a board redesign is possible that you upgrade to Channel Link II and try a device like the DS92LV2411/DS92LV2412, which also supports 24-bit Color. However, you will need to use a different input interface, as all the lines are serialized onto one CML differential pair for Channel LInk II.
Thanks,
Michael
Hi Eli,
FPD Link I devices do not have much capability to assist in minimizing EMI like those seen in the later generation devices. All it offers is the low LVDS voltage swing, which helps reduce EMI when compared with RS-422, PECL, and TTL.
You will find more particular features to reduce EMI in the next generation of Ser/Des products (Channel Link II or III). For example, to reduce EMI in the DS92LV2411/DS92LV2412, the deserializer has SSCG, output slew rate control, and data randomization/scrambling.
Thanks,
Michael
Hi Eli,
Due to the nature of LVDS signaling, FPD-Link I devices are typically low EMI products if the PCB is designed properly. Here are some typical high speed design practices to reduce EMI:
Mike Wolfe
DPS APPS / SVA