Other Parts Discussed in Thread: TLK110
Hi,
The TLK110 is not entering into parallel detection when link partner ANEG capability is disabled.
Experiment 1:
1. In link partner ANEG is diabled.
2. In TLK phy, Write 0x3300 in to basic control reg to restart aneg.
3. wait for some delay,
4. Read basic status register, got 0x7869. Where link is not up.
Here i am expecting parallel detection should happen and it has to enter into Half duplex with link detected.
But after power on ,Just i read basic status register. The link was up.
Experiment 2:
1. Aneg is disabled at link partner.
2. Power ON TLK, wait for some secs
3. Read Basic status register, got 0x786d, here link is up.
Parallel detection would have happened above.
Can you help me to sort it out why parallel detection not happened with Experiment 1?