Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO3088 - RS485 transceiver - external wiring between two ISO3088 without GND2

Other Parts Discussed in Thread: ISO3088

I have two equipments, separated from 600m, equipped with ISO3088 RS485 transceivers. The link of communication between them consist of a cable composed of only two wires.

Can I use one wire for the output A+ and the other wire for the output B-, without to connect the GND2 ?

In fact, How could we connect these two transceivers with only two wires ?

Thank you.

Gérard TRIC