Other Parts Discussed in Thread: SN65CML100, SN65LVCP1412, DS15BA101
Hello,
I require a level translation for a 100 ohm 1GBPS LVDS serialized output (VOD=350mV) to a SFP module which requires a minimum VOD of 500mV. The SFP input is internally AC coupled and has a 100 ohm internal termination.
Is there a TI device which can take a 350mV differential signal and drive a minimum of 500mV into a 100 ohm terminated load? ie The SN65CML100 only generates 400mV into 100 ohms.
Thanks
Mitch