Other Parts Discussed in Thread: SN75DP139
Hi, SN75DP139 datasheet has listed 4k x 2k (30Hz, 24 bpp) in the Features list. Does it really work at 4k x 2k (30Hz)?
Please verify. Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Yes it does.
Regards,
Diego.
Hi Diego,
Thanks for the reply. What kind of DisplayPort ++ (dual mode) source do you use for 4K? Can you name the graphic card or configuration for source? I am trying with most of the cards and PC/laptops/Macs currently result is only 1080p highest. Thanks.
Hello,
We do not have information regarding an specific 4K source, all the tests for this device were done by means of a general purpose generator/analyzer (ParBERT). However you can try with AMD/GEFORCE graphics cards, I am pretty sure they have products supporting 4K resolution.
Best regards,
Diego.
I have tested with AMD graphic cards including latest chipset which support 4K. I have tested with various PCs and Mac which supports 4K resolution on DP. Only got 1080P came out with this chip.
This chip can go up to 3.4Ghz when testing with (BERT). I agree with Diego. I have tested myself.
But it can not send the correct signal from DDC line to the DP++ source to pass the 4K, 30 Hz resolution.
I believe the TMDS connector identification LOGIC BLOCK in this chip is only good for 1080p. Can you please check with factory and confirm?
BR,
Hello,
I will confirm with the design team. In the mean time, Could you confirm tthe status of I2C_EN and DDC_EN?
Best regards,
Diego.
DP139 is a Dual Mode Type 1 device. VESA released a new Dual Mode standard and defined a new Dual mode type called Type 2. According to this new standard, a Type 2 device supports up to 300Mhz clock and a Type 1 device supports upto 165MHz clock. If source software check for Type 2 in order to enable 4K2K video, then the DP139 will not work. Even though DP139 supports 4k2k, it doesn't have the Type 2 identifier and source will not enable higher than 168MHz.