Other Parts Discussed in Thread: DS92LV16
Hi,
I am using DS92LV16 for a SERDES project. The board use DS92LV16 only for deserliaze a 16bit bus, in this case I need only the RX part of the chip. As I Know the TX and RX are completely separated PLL too (TX_RX). On the pin table PLL poer pins are called with the same name PVDD (30-31 and 75-77) e PGND (29-32 and 74-76) I am not able to understand which are for TX part and RX. I need to power only the RX part (Deserializer). I suppose it's correct to power only the part I am using, am I right.