This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83848I / unused pins connection

Guru 20090 points
Hello,
 
Could you please let me know the connection of below unsed pins?
Can we float these pins ?
 
-7pin (PWR_DOWN / INT)
-8,9,10,11,12 pins (JTAG Interface)
-25pin (25MHz_OUT)
-27pin(LED_SPEED/AN1)
 
And is VIH of PWR_DOWN/INT 2V(min) ?
 
Best Regards,
Ryuji Asaka