This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83848I / Ceramic capcitor for PFBOUT

Guru 20090 points
Hello,
 
In the datasheet page 14, there is PFBOUT description as "output Parallel caps, 10μ F (Tantalum preferred) and 0.1μF, should be placed close to the PFBOUT. Connect this pin to PFBIN1 (pin 18) and PFBIN2 (pin 37)".

Can we use ceramic capacitor for this 10uF output cap ?
Since I believe that Tantalum caps need for stability, ceramic capacitor is accepted if we added series resistor.
If yes, please let me know the resistor value for keeping stability with ceramic cap.

Best Regards,
Ryuji Asaka