Hi,
Our customer is looking for the devices that meet Standard RS422(V.11).
Please let me know if there are the devices that have much shorter propagation delay time(tPLH,tPHL)
than AM26LV31E/AM26LM32E.
Best Regards,
Kato
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Toshiyuki-san,
SN65HVD05 is faster but just 1TX/1RX channel.
What is their data rate? AM26LV31,2 is fast enough.
Ronald - san,
Thank you for the reply.
Our customer's data rate is 40Mbps.
Best Regards,
Kato
Kato-san,
40Mbps is not supported by V.11 which is a 'up to 10Mbps' standard.
When used at 10Mbps it should be V.11 compliant. However, I have not carefully compared it to all the V.11 specs.