Other Parts Discussed in Thread: SN65MLVD048, SN65LVDS104, SN65LVDS048A
Hi Team,
Could the SN65MLVD048 be used with single standard LVDS backplane signal as input(s)?
Other recommendations? We seem to make 1:4 the other way.
Thanks, Dan
From: Patrick.Lindo@L-3com.com [mailto:Patrick.Lindo@L-3com.com]
Sent: Wednesday, January 27, 2010 11:11 AM
To: Faluade, Loretta
Cc: Lindo, Patrick @ AED
Subject: Help 1:4 LVDS to LVCMOS/LVTTL IC
Hi Loretta,
Maybe you can help me with this request, I am working on a project and need a 1:4 LVDS to LVCMOS/LVTTL IC. I have a +3.3V LVDS clock signal (40MHz) coming into the board that needs to go to 4 components that have single ended LVCMOS inputs. I am hoping to find a component that does this.
Patrick Lindo
Hardware Engineer
L-3 Communication
Aerospace Electronics
One Wall Street, First Floor
Burilington, MA 01803
781-270-2142