Other Parts Discussed in Thread: SN65LVDS2, SN65LVDS1
Hi,
Can SN65LVDS1 & SN65LVDS2 be used for point-to-point clock distribution?
Thanks,
M
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Mohammed,
Yes the SN65LVDS1 and SN65LVDS2 can be used in a point to point clock distribution application. What is the input to the SN65LVDS1 going to be (i.e. TTL, LVTTL, LVCMOS)? Do you need to fan this clock out in your application to multiple devices on your board? I can recommend some fan out buffers for you.
Regards,
Michael Peffers
High Speed Interface Applications
Hi Michael,
Thanks for your reply.
SN65LVDS1 will be driven from an LVCMOS oscillator (24MHz). The clock is needed at only one device (CPLD), so I don't think there is a need for a fan-out buffer.
Regards,
Mohammed
Hi Mohammed,
Can we close this post out or will you be following up with more questions about the SN65LVDS1 and SN65LVDS2?
Regards,
Michael Peffers
High Speed Interface Applications