Will the PCA9306 chip be damaged if Vref2 is connected directly to 3.3v?
Note Vref1 is tied to 1.8v.
We have since reworked the cards to tie pin 7 & 8 together and using 200K resistor up to 3.3v and most are operating with no problems, but a few cards are having an issue with this bus.
We continue to investigate, but were wondering if the chip could have been damaged due to the incorrect connections.