We are using two PCA9306 devices for I2C level translation on OMAP3503 application and I notice the PCA9306 is dumping 21- 27ma current into the 1.8V rail.
It is translating from 1.8V logic to 3.3V logic.
I have 1.1K pullup on SDL and SDA lines to 3.3V and 4.7K pulllup on the 1.8V logic side.
I have confirmed that current is flowing apparently from the 3.3V rail to the 1.8V rail this by lifting the Vref1 pin and measuring the current and noticing it is traveling from the chip back to 1.8V. I have disconnected the IC's on the 3.3V side of the SDA and SCL so there is only the resistor pullups. I ahve verified the resistance values of the pullups
This causes a problem for the switching power supply when the system is beginning to come up since the power draw on the 3.2MHZ swticher on TPS65920 is much less than 21 ma when first powering up. This causes the power supply to rise to over 2.0V.
Any thoughts why the PCA9306 would be dumping current to the 1.8V rail?