Other Parts Discussed in Thread: SN75DP130
Hi,
We are using the SN75Dp130 evaluation board. I have connected a DP1.1a source at input at 1920 x 1080 resolution, but the output comes at 1024 x768 resolution. SHould we need to adjust any parameter - there is no provision on the board to adjust except few jumpers which are not related to resolution - can anybody help me on this. The I2C interface is active as the U5 IC is not mounted on the board.
thanks
Harikrishna