Other Parts Discussed in Thread: DP83848I
Best Regards,
Ryuji Asaka
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: DP83848I
Hello,
We do not recommend using resistor values other than the values listed in the datasheets and design guidelines.
Regarding the value of RBIAS, 4.87K ohm resistors must be used.
Thanks,
John
Ryuji-san,
The IEEE 802.3 specification defines the required 100BASE-TX VOD (Voltage Output Differential). Per the specification, this voltage must be 1V +/-5%.
The value of the RBIAS resistor and the termination resistors for RD/TD have a direct impact on this output voltage. If these vary by more than 1% from the stated datasheet values, compliance to the 100BASE-TX VOD cannot be guaranteed.
Patrick