Other Parts Discussed in Thread: SN65LV1224B, SN65LV1023A
Hello,
I use SN65LV1023A serializer and SN65LV1224B deserializer on two PCBs. Both ICs are connected with each other over optical cable (1.25 Gbps) with SFP connectors. Reference clock is 50 MHz on both sides.
I lock using 1111100000 patterns successfully. I use the same pattern when the line is idle. Data transmission is also good. However sometimes some data is sent wrong or lost. This happens very rarely, sometimes once a week.
In the datasheet it is written:
"Notice that the RMT pattern only affects the deserializer lock time, and once the deserializer is in lock,
the RMT pattern does not affect the deserializer state as long as the same data boundary happens each cycle."
Does this mean that the error is not related with my data pattern?
Where can be the error?
Regards,
Ersin ÖZALP