Other Parts Discussed in Thread: TUSB2077A
I am debugging a product and I've noticed two things using the TUSB2077.
1. On power up the microprocessor and TUSB2077 don't intialize 100% of the time. It is more like 90% of the attempts from power up. When the microprocessor lets go of the reset of the TUSB2077 and they don't initialize correctly, the HUBCFG and PORTPWR indicators blink once or muliple times red and then stay red. Any hints on how to get these to initialize correctly 100% of the time?
2. On power up in the 90% where everything initalizes fine. I have a USBHID device enumerate correctly with my microprocessor through the TUSB2077. When the reset of the USBHID device is pressed, the USBHID device will attempt to reattach to the microprocessor. During the time the USBHID tries to reattach, the PORTDIS light goes red. Any ideas why on power up this will work and not during a reset condition?
Thank You for Your Time,
Colin