Other Parts Discussed in Thread: TLK105L, DP83640T-EVK
Hi.
I will need to mount my Ethernet as follows:
1) A "standard" pc board will have MAC, TLK105L and PHY-side termination components.
2) A "personalized" pc board will be populated with two versions:
- version ONE with twisted pair connector + transformer + transformer-side termination components and
- version TWO with optic fiber transceiver + transceiver side termination components.
The question: can I use the SAME termination circuit in the standard board for the two personalized versions? Although the commonly recommended circuits are different for each case, I think that it will be ok if I use
- for TD pair: 50 Ohm to 3V3 bias;
- for RD pair: 130 / 80 Ohm bias OR ELSE 50 Ohm to 3V3 bias with capacitor decoupling from fiber transceiver.
Can I do that? What termination is better for RD pair
Regards.
Christos