Other Parts Discussed in Thread: XIO2213B, XIO2213BEVM
Hello,
What is the maximum recommended length of the differential 1394b traces for the XIO2213B?
I saw there was a 20-inch recommendation for the PCI-E traces in the Implementation Guide, but have heard conflicting numbers on the 1394b, as short as 0.8 inches. The 1394b traces on the XIO2213BEVM look to be at least 2.5 inches. On a new design using the XIO2213B, we are looking at a max 1394b trace length of 5 inches, but wanted to make sure this wasn't outside the expected bounds.
Thanks,
Jonathan Bender