Other Parts Discussed in Thread: LMH0046, LMH1218
I've posted a similar comment as a reply elsewhere, but this seems more to the High Speed Interface Forum. When I examine the jitter on the output of this reclocker board it doesn't seem much better than the input.
The conditions I am have are:
Jumpers as per User Guide.
SMPTE 292 SDI input (colour bars test pattern with excessive jitter)
Carrier detect LED is lit.
1.485Gbps LED is lit.
Fault LED on LMH0309 (sic) is lit.
SDO output measured 2us downstream of trigger point shows ~0.5ns jitter (should be better than 130ps)
Is the reclocker chip in bypass mode, somehow?