Other Parts Discussed in Thread: DP83848I, ALP
Hi,
I'm using a DP83848I in-conjunction with the 9th MAC of a KSZ8999 switch. The DP83848I is the host port which connects to my LAN. The remaining 8 ports of the KSZ8999 are for system devices. I can sometimes ping a device which is plugged into any of the ports of the KSZ8999 but its very intermittent. The LINK LED attached to the DP83848I is flashing continuously @ approximately 6Hz when a network cable is plugged into the port. The ACTIVITY LED is off. Without a network cable attached the LINK LED is off.
The DP83848I is configured as: LED MODE 2, MII MODE. RBIAS is 1.2V and the PFBOUT pins are 1.78V. The MDIO pin has a 2k2 pullup.
What does the flashing of the LINK LED indicate? Has the PHY been configured incorrectly?
The same LINK LED behaviour can be seen on all the prototype boards I have tried so its unlikely to be a faulty IC. I have even removed the KSZ8999 from the circuit and the same LED behaviour on the port connected to the DP83848I can be observed.
Thanks for the help.