Other Parts Discussed in Thread: DS32EL0421, TLK6002
Hi,
I am trying to implement a SERDES (SCAN12100,TLK6002, DS32EL0421, or something similar) to serialize a 20 bit, 100MHz parallel input to 6.25Gbps. I have an Altera DE 4 board with a STRATIX IV, and I would like to interface it with one of these chips. First of all, how do I make sure that my FPGA can definitely be interfaced with these chips? For example, how do I know which of the chips is most compatible with my board.
Secondly, I do not have experience or expertise in designing these boards. I was wondering if you could suggest any assembly company that help solder the chip on the pcb.
Thank you very much in advance.