Other Parts Discussed in Thread: TUSB2036
Hello Team,
My customer is making a small card called as BB Adapter with two USB ports and power supply circuitry including a battery charging Circuit.They are planning to use a USB Hub that will detect the different system states and control the current taken from PC and for that downstream port HUB TUSB2036 is being considered.There will be two USB ports : One for normal USB connection to connect any device like Memory Card Reader ,hard disk etc. another USB port will be either connected to PC or to an external power Adapter i.e.additional requirement to support battery charging from the external USB Power Adapter (instead of PC USB port).In that case what will be the state of SUSPEND pin. External USB Power Adapter will have D+ and D- lines shorted with 200Ohm resistor and only 5V power and Ground will be available.If the SUSPEND output is active then it will disable the charging circuit and we will not be able to charge from external USB adapter.
Also,apart from the throughput differences what can be other design challenges faced when the system has the USB1.1 and we plug in USB2.0 HUB.
Please let me know if you have any questions further to be more clear on the query stated above.
Thanks and Regards
Bijeta Chakraborty