Other Parts Discussed in Thread: SN6501, ISO1176, ISO1176T, PROFIBUS
I compared the datasheets and application notes for both parts and wonder if the ISO1176T is basically a ISO1176 with integrated SN6501 or whether the transformer driver is different?
The transformer ratio for 3.3-5V is specifiied as 1:2 for the SN6501, however it is 1:2.2 for the ISO1176T. So it appears that different transformer are required hinting a different transformer driver circuit in the ISO1176T.
We intended to use the Midcom 760390015 (1:2) (which is the recommended part for the SN6501) in conjunction with the ISO1176T.
Has the Midcom 760390015 been tested/validated for the ISO1176T?