Other Parts Discussed in Thread: TMDS361B
Hi Team,
I had posted the following topic in the past, however, could you please let me ask you again about the clock detection function and HDMI compliance testing ?
TMDS361B - HDMI Compliance Testing
http://e2e.ti.com/support/interface/digital_interface/f/130/t/300191.aspx
[Question1]
I believe that the reason why TMDS361B cannot pass HDMI compliance test by clock detect feature ENABLED is because there is no 50ohm pull-up to VCC when there is NO input clock. The device would not be able to satisfy the requirement of TMDS termination voltage; TMDS pin voltage = AVCC+/-10mV.
First of all, is my recognition correct ?
[Question2]
If my recognition of Question1 is correct, I thought that by adding 1kohm resistors to each TMDS+/- would pull-up each TMDS pin voltage to VCC. Do you think the following schematic would be able to pass the HDMI compliance test enabling clock detect feature ?
Can you recommend these pull up resistors ?
I am grateful for your help.
Best Regards,
Kawai