Other Parts Discussed in Thread: LMH0302, LMH0384, LMH0387
Hi,
I need to know if the output of LMH0302 is a real 3-state when chip is disabled (ENABLE = GND).
Bye
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Stefano
The easiest way to think of the output of the LMH0302 is like a CML output (looks like a differential pair with a current source on the emitter tail). When the chip is disabled, the current source is turned off, when enabled there is a current sink from one output or the other. A 'real 3-state output' would have high output impedance when disabled, and low output impedance when enabled, the LMH0302 always has a high output impedance (current source), and the output impedance is set with the external load resistors.
Mark
Thank you Mark,
I'm thinking about putting toghether a cable driver and a cable equalizer (LMH0302 and LMH0384) on the same BNC connector...I don't need to be really 3G-SDI compliant. Do you think it's possible?
(I know it could be best done with the LMH0387, but I'm trying to use more standard components).
Stefano
It is possible, but very difficult, especially if you need/want to meet the SMPTE return loss specs for the connector - I would strongly encourage you to use the LMH0387 which was designed especially for this purpose - and the cost should be lower than for the LMH0302 and LMH0384 combined.
Mark