Other Parts Discussed in Thread: TUSB2036
Hallo,
Can the TUSB2036 use 6-MHz external oscillator source when MODE is low?
When MODE is low, the TUSB2036 is internal APLL mode and uses 6-MHz crystal between XTAL1 and XTAL2 as the fundamental frequency.
Instead of the crystal, when MODE is low, can 6-MHz external oscillator source is used inputting to the XTAL1 and leaving the XTAL2 open?
Best Regards,
Kazu Ogawa