Other Parts Discussed in Thread: ULN2003A
It appears that then maximum input voltage for any given input is 24VDC, What is the maximum input current ? is a series resistor required ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Bob,
Input voltages up to 30V are allowed. However high input voltage causes more internal power dispassion (heating). Pd=VIN*IIN. A series resistor is helpful to reduce power dissipation.
Bob,
The nominal input impedance is 2.7k ohms terminated at 1.4V.
To drop 24V to 5V. RIN=2.7k*(24V-5V)/(5V-1.4V) = 14.3k