Other Parts Discussed in Thread: DS90CF386
Greetings,
I am currently working on an embedded computing application that requires a small form factor computer and touchscreen. The computer has an Intel atom processor with native LVDS output. I am using a DS90CF386 LVDS Receiver chip to convert to 24-Bit TTL signals for a 5.0" Flat Panel Display. The problem is the display is not working - the best I can get is random vertical lines on the display. When I look at the TTL signals to the display it looks as if the VSYNC, HSYNC, and DEN signals are all inverted? This is with a CLK input signal of about 32MHz. However, if I slow the CLK signal down to about 24MHz by changing the default screen resolution in BIOS to 640x480 (which is not the correct resolution for the LCD) the VSYNC, HSYNC, and DEN signals now appear correct? (I still get garbage on the LCD though).
Any ideas on why the signals would be inverted at the faster clock speed? Is this a clue that something else is off? Any advice on LVDS to TTL interfaces in general?
Thanks much in advance.
-Chris.