Other Parts Discussed in Thread: SN65HVD1781
Hi,
I'm using a RS485 transceiver (SN65HVD1781) which is +/-70V fault-protected.
Our device must meet the IEC 61000-4-2 standard so we thought about adding a TVS protection.
For example, a SM712 TVS (+12V/-7V), but I pressume that it would burn if an overvoltage fault occur.
What TVS I would have to choose to maintain the fault protection?
Thanks,
Pablo